Homepage

Diashow Stage

Musiktheater Bielefeld

At the end of the theatre season 2003/2004 the theatre, which was built in 1901, was more...

Stage

DRIVE SOLUTIONS FOR GREAT EVENTS

Stages in community halls, theatres and opera houses require safe, reliable and quiet drive technology. Curtains, podiums, rotating, lifting or sliding stages and stage structures must be brought into the correct position unnoticed by the audience and without endangering the actors and stage hands.


For these applications the trend is towards electromechanical drive systems as these are more suitable than relatively complex, high-maintenance hydraulic drives, especially where space is restricted. As compact and cheap alternatives to hydraulic drives, they have proved themselves above all for raising and lowering loads on the stage. For more than 45 years, NORD DRIVESYSTEMS has been at home in almost every branch of industry where transportation solutions are used for internal logistics. Our drive components and systems are essential wherever things need to be moved, because all movement needs drive - as efficiently and safely as possible. Because of this, we provide the entire spectrum of mechanical, electrical and electronic drive technology from a single source, from motors and gear units to central and decentralised control technology.